FRDMK64 FTM2 Ch0 config problem with PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDMK64 FTM2 Ch0 config problem with PE

1,237 Views
therealfreegeek
Contributor IV

Hi, I am using the FRDM K64 with KSDK1.3 and am trying to set up FTM2 Ch0 as an output but get an error from PE.

 

You can see from the image below I have selected the pin to be routed to J1-1 which is Port B18.

 

141823_141823.jpgftm2 A.jpg

 

I then try to select the pin direction as an output and get this error.

 

141860_141860.jpgftm2 B.jpg

 

Is this a bug or am I doing something wrong?

 

Thanks

Jim

Labels (1)
3 Replies

1,066 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello JIm,

I create one simple project to have a test , it can work well on my side,

and the attachment is my project ,you can test it on your side , it it can work well,

please create one simple project to have a try , or you can also send your project to me , i

will check it on my side .

pastedImage_0.png

Hope it helps

Alice

1,066 Views
therealfreegeek
Contributor IV

Hi Alice,

Thanks for the offer, however I closed the project, removed it from the workspace and imported it again, the error then disappeared.

Thanks

Jim

0 Kudos
Reply

1,066 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

OK Jim, welcome !

0 Kudos
Reply