FRDM KL25Z : board no more listed in  KDS 3.0.0

cancel
Showing results for 
Search instead for 
Did you mean: 

FRDM KL25Z : board no more listed in  KDS 3.0.0

Jump to solution
455 Views
Grandpierre
Contributor II

Hi,

I have googled everywhere before posting.

In my updated KDS 3.3.0 with Processor Expert for Kinetis to 3.0.1 update : there is no support for my FRDM KL25Z (only FRDM-K22F, FRDM-K64F, FRDM-K46Z and several TWR).

How to get it supported ?

(I see that previous version supported it : Freescale Freedom development platform: Freesca... | element14

Thanks

Labels (1)
0 Kudos
1 Solution
231 Views
DavidS
NXP Employee
NXP Employee

Hi Thierry,

You are correct the FRDM-KL25Z board not supported when not using KSDK_1.3.0 but if you choose the Processor it is.

If you do File->New->Kinetis Project and then after naming the project, go to the "Processors->Kinetis L-> MKL2x->KL25Z->MKL25Z128xxx4 " the project will be created for PE support without KSDK_1.3.0.

Regards,

David

View solution in original post

0 Kudos
1 Reply
232 Views
DavidS
NXP Employee
NXP Employee

Hi Thierry,

You are correct the FRDM-KL25Z board not supported when not using KSDK_1.3.0 but if you choose the Processor it is.

If you do File->New->Kinetis Project and then after naming the project, go to the "Processors->Kinetis L-> MKL2x->KL25Z->MKL25Z128xxx4 " the project will be created for PE support without KSDK_1.3.0.

Regards,

David

0 Kudos