I have the FRDM-KL05Z board but when I want to create a new prject my borad is not in the list. Is it possible to update the list of boards?
Solved! Go to Solution.
Hello Gerard:
The boards you see in that list are only those supported right now by KSDK. Kinetis SDK is a software driver platform for Kinetis MCUs. Only those boards are supported right now. For details check Software Development Kit for Kinetis MCUs|Freescale.
If you have a FRDM-KL05, then as Iva mentioned you can select the MCU from the Processors list. With this you can create a baremetal project or baremetal + processor expert project.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Gerard.
Please, go to File > New > Kinetis Design Studio Project > and go to Processors
Iva
Iva,
When I want to select a device there is board folder with two FRDM (K22F and K64F) but not the FRDM-KL05Z.
Is it possible to update the board folder with the FRDM-KL05Z?
Thanks,
Gerard
Hello Gerard:
The boards you see in that list are only those supported right now by KSDK. Kinetis SDK is a software driver platform for Kinetis MCUs. Only those boards are supported right now. For details check Software Development Kit for Kinetis MCUs|Freescale.
If you have a FRDM-KL05, then as Iva mentioned you can select the MCU from the Processors list. With this you can create a baremetal project or baremetal + processor expert project.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Gerard,
No. It is not possible.
It is support for boards - FRDM-KL43Z, KV30 and K02 devices, TWR-K24F (you can import it from Software Development Kit for Kinetis MCUs|Freescale
and the boards, which you see in the list.
So, choose the choice Processors > Kinetis L > KL05Z
Best Regards,
Iva