我将刚拿到的FRDM-K66F开发板按FRDM-K66F|Freedom开发平台|Kinetis MCU|恩智浦
利用自带的micro-usb电缆接入PC(win7 32bit)后,安装mbedWinSerial_16466.exe,出现。放弃。
然后,按照SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2 里的顺序安装Setup_JLink_V510u.exe,先后试了4.68 5.02 5.10 5.12几个版本,也无法使板子被pc识别。
如今项目非常紧。需要调试程序,而所有的下载调试工具,均不能正常使用,请提供帮助,谢谢
Hi,
FRDM-K66 use OpenSDA v2.1 interface, please refer this document to see if it can help
Summary of FRDM-K22F debug interface
seem there is no P&E open sda firmware interface released yet, but you can refer Jlink and mbed parts.
Can this help you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------