Error using Differential and Single-Ended ADC Channels in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error using Differential and Single-Ended ADC Channels in KDS

ソリューションへジャンプ
1,357件の閲覧回数
brycelembke
Contributor III

I have a need for both differential and single ended channels. When I use the ADC component from the component library and set some channels to be differential and some to be single-ended, I get the error 'Combining Differential and Single-Ended channel modes in A/D channel list required native result data format'. I have tried changing the Result Type, but I always get this error. Is there a way in KDS to use both Differential and Single-Ended channels on the same ADC? (My hardware is already spun, so it would be difficult to use the other ADC block).

I am using a K10DN512VLL10 with KDS 2.0.

 

Bryce

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,168件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bryce,

In the "Result type" , please configure as this :

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,169件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bryce,

In the "Result type" , please configure as this :

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,168件の閲覧回数
brycelembke
Contributor III

Perfect, that is what I needed.

0 件の賞賛
返信