Error in KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in KDS

799 Views
donad
Contributor II

Hi,

When I run aprogram in KDS ,the following error shows up.

"The target endianness is set automatically (currently little endian) "

Why does this error occur? Please help.

 

Regards,

Dona

Labels (1)
0 Kudos
Reply
1 Reply

719 Views
BlackNight
NXP Employee
NXP Employee

Hi dona,

can you shar a screenshot? I believe this is a message coming from the Segger J-Link debug firmware, and is not an error, but an information message. You can tell the Segger J-Link GDB server if it shall use little or big endian, and by default the firmware selects it automatically based on the device used, which is little endian for ARM.

I hope this helps,

Erich

0 Kudos
Reply