Error debugging KE04Z in KDS 3.2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error debugging KE04Z in KDS 3.2.0

989件の閲覧回数
jessaskey
Contributor I

Hi there...

 

Im running KDS 3.2.0 under Windows 10 along with a KE04Z. My first program is to flash the Blue LED every 1 second. I have a Processor Expert project set up, debugging configured with my Device showing on USB in the Debugging config ( USB1 - OpenSDA), the FRDM is running the debug app (DEBUG-APP_Pemicro_v107.SDA - Solid Green LED ). When I Run my Debug Configuration.. I get this output...

 

Initializing.

Target has been RESET and is active.

CMD>CM D:\Freescale\KDS_v3\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.3.6.201602211227\win32\gdi\P&E\supportFiles_ARM\NXP\KEx\freescale_ke04z128m4_pflash.arp

Initializing.

Initialized.

;version 1.03, 06/02/2014, Copyright 2014 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [ke_128k_pflash_ftmre_m0]

;device freescale, ke04z128m4, pflash

;begin_cs device=$00000000, length=$00020000, ram=$20000000

Loading programming algorithm ...

Error loading .ARP file : D:\Freescale\KDS_v3\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.3.6.201602211227\win32\gdi\P&E\supportFiles_ARM\NXP\KEx\freescale_ke04z128m4_pflash.arp at address 1FFFF000

Error loading programming algorithm - load aborted.

Error occured during Flash programming.

 

However, I have verified that the .arp file above exists in the location.

 

Is this a permission issue since Im on a different drive? Windows 10 issue? Other issue?

 

Anyone have any hints?

 

thank you!

Jess

ラベル(1)
0 件の賞賛
返信
1 返信

829件の閲覧回数
jessaskey
Contributor I

okay, I think I have this solved so I will post here the answer in case it helps anyone else...

When I had set up my Processor Expert Project, I had selected the KE04Z128M target MCU as that was what I thought I was going to use originally. When I switched over to the FRDM-KE04Z, I neglected to change my target device to the KE04Z8M4.

Once I made sure that the Target Device (inside of Debug Configurations, Debugger Tab, Select Device) matched my development board, I was able to successfully download my image and debug.

0 件の賞賛
返信