Erase flash FRDM-K64F with KDS 3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Erase flash FRDM-K64F with KDS 3.0

Jump to solution
1,120 Views
pablofonovich
Contributor II

Hi:

I'm using KDS and uTasker O.S with FRDM-K64F... I set a fixed IP to the board and used it as a webserver with no problem... But if i change that IP, compile and flash again wid KDS and J-Link, the old IP remains... the same happens with the html files i loaded to it...

 

Using uVision, is possible to workarround this problem by erasing the device with the erase button of that IDE, but i cannot find a simple way to do it with KDS 3.0

Is there any function similar to uVision's erase?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
708 Views
pablofonovich
Contributor II

Hi:

I've finally solved this... I just created a project for the board that fills the text region of memory with 0xff... i found something similar in a forum and it worked

View solution in original post

1 Reply
709 Views
pablofonovich
Contributor II

Hi:

I've finally solved this... I just created a project for the board that fills the text region of memory with 0xff... i found something similar in a forum and it worked