Equivalent for derivative.h in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Equivalent for derivative.h in KDS

ソリューションへジャンプ
2,156件の閲覧回数
georgschmidt
Contributor III

Hi,

 

I installed KDS today and I'm trying to migrate my MK60-Project from CodeWarrior to KDS.

The project wizzard of CW did create a header-file "derivative.h" which just includes the controller specific header-file (MK60F12.h in my case) in which the memory map and all the peripheral registers were defined.

Is there an equivalent for this in KDS?

 

Regards,

Georg

ラベル(1)
0 件の賞賛
返信
1 解決策
1,847件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Georg,

have a look in

C:\Freescale\KDS_1.0.1\eclipse\ProcessorExpert\lib\Kinetis\iofiles

Regards,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,848件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Georg,

have a look in

C:\Freescale\KDS_1.0.1\eclipse\ProcessorExpert\lib\Kinetis\iofiles

Regards,

Erich

0 件の賞賛
返信