As far as I can tell, TWR-KL25Z48M is not yet supported by KSDK 1.1.0 (using KDS 2.0.0).
Any timeline on when this will be available?
Currently it seems that there is no source-level project available for this board using KDS/GCC (the only packages I have found which do contain source are either for CW or are set up for another compiler.) I am currently trying to get a project building with Processor Expert but it would be nice to have a fully supported official package to start from.
Hi phil,
kl25 should be supported in KSDK 1.2GA, and it will be available in Apr.2015
Best Regards,
Zhang Jun
============================================
this answer is for you, if it helps, please click on "Correct Answer " button. thanks!