ERROR: This component is not supported in Kinetis SDK project mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR: This component is not supported in Kinetis SDK project mode

648件の閲覧回数
armaram
Contributor III

While adding a component from component library to the project (BitIO) I get this error.

We are trying to generate code from processor expert on KDS v3.0.0.

Would anyone know what mode are we supposed to use to avoid this error?

ラベル(1)
0 件の賞賛
返信
1 返信

466件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If you have created a project with the Kinetis SDK enabled, then all the non-SDK components (with a few exceptions) don't work. You need to use the components starting with "fsl_" in the name if you are using the Kinetis SDK.

Otherwise: Overview: Processor Expert gives an overview about the different component types.

I hope this helps,

Erich

0 件の賞賛
返信