EEPROM WITH KINETIS PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM WITH KINETIS PE

ソリューションへジャンプ
2,120件の閲覧回数
marceladuenas
Contributor II

Hi everyone, i need to play with an eeprom , the 24LC512; i am using the mkv31f256vlh12 . I know that the compenent exist into the processor expert selection , and i need an i2c conectivity but i dont know how can i configure the settings and test . Some body can help me...

ラベル(1)
1 解決策
1,891件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

do you mean this driver: Driver for Microchip 24xx Serial EEPROM | MCU on Eclipse

?

I don't have any KV device, but I have used that Microchip EEPROM for other devices. But the project needs to be for Processor Expert, *without* the Kinetis SDK, as the Kinetis SDK is not compatible with that driver.

I have an example of it for CodeWarrior with Processor Expert here: mcuoneclipse/Examples/FRDM-KL25Z/FRDM-KL25Z_24LC_EEPROM at master · ErichStyger/mcuoneclipse · GitHu...

I hope this helps,

Erich

元の投稿で解決策を見る

2 返答(返信)
1,892件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

do you mean this driver: Driver for Microchip 24xx Serial EEPROM | MCU on Eclipse

?

I don't have any KV device, but I have used that Microchip EEPROM for other devices. But the project needs to be for Processor Expert, *without* the Kinetis SDK, as the Kinetis SDK is not compatible with that driver.

I have an example of it for CodeWarrior with Processor Expert here: mcuoneclipse/Examples/FRDM-KL25Z/FRDM-KL25Z_24LC_EEPROM at master · ErichStyger/mcuoneclipse · GitHu...

I hope this helps,

Erich

1,891件の閲覧回数
marceladuenas
Contributor II

I have a question the data stored where can i see?, the data read is stored in reg? or how can i verify the data stored and read it, in the debug mode.

thank you for your help

0 件の賞賛
返信