Does KDS have tutorial for application of demo project for TWR-K70F120M and TWR-LCD-RGB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does KDS have tutorial for application of demo project for TWR-K70F120M and TWR-LCD-RGB?

1,888 Views
draganstanic
Contributor I

I just got my hands on TWR-K70F120M-KIT and TWR-LCD-RGB. Also trying KDS firs time.  Went thru online DVD and online documentation and could not find an working example wolk true for KDS.   Tower in"TWR-K70F120M Quick Start Demo - Lab Guide for MQX 3.8" under " 5 Development Software and Programming the Board" has only example for IAR development environment".  Is there comparable walk-true for KDS?

 

Thanks

Dragan Stanic

Labels (1)
0 Kudos
Reply
4 Replies

1,395 Views
towerer
Contributor III

any news to this?

0 Kudos
Reply

1,395 Views
ghemstreet
Contributor II

KDS does support that chip, but I don't think there is currently a board configuration (.peb file) for the TWR-K70F120M.  You can create either a bareboard project or use Processor Expert for this board. There are tutorials on-line for using Processor Expert but I don't think they are specific to K70...

0 Kudos
Reply

1,395 Views
michelebacchere
Contributor I

There are any news with KDS 3.0 and TWR-K70 board compatibility? Any tutorial to migrate from CW+MQX project and new KDS 3.0 project?

0 Kudos
Reply

1,395 Views
GregErman
Contributor I

I'm resurrecting this thread in hopes that there has been some development.

Does anyone have working code for this setup that they could share?  Specifically for KDS and preferably freescale's eGUI ( if not PEG ).

Any help would be greatly appreciated.

Thanks in advance.

0 Kudos
Reply