Demo project of fatfs with KSDK 1.0.0 and PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Demo project of fatfs with KSDK 1.0.0 and PE

1,820 Views
giacomopetrini
Contributor IV

I can't find any demo project using the fatfs (and sdhc) provided inside KSDK 1.0.0.

 

Somebody has something that can share about it?

 

Thanks Bye

Giacomo

Labels (1)
0 Kudos
Reply
5 Replies

1,519 Views
intractablesubt
Contributor III

I asked a similar question here: How do I connect a fsl_sdhc component in to MQX?

No one has offered an answer.

0 Kudos
Reply

1,519 Views
giacomopetrini
Contributor IV

Have you watched the tutorials?

http://www.freescale.com/webapp/sps/site/training_information.jsp?code=WBT_MQX_RTOS_COURSE&tid=vanmq...

There is one on datalogging, maybe it could help.

Or this:

http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/

you need to download the needed PE components from sourceforge (the link is in the comments of the tutorial).

The guy who wrote the tutorial (Erich Styger)  write in this forum too.

Please let me know if you manage to use SDCH and MFS with MQX, I'm interested in the thing.

Best Regards

Giacomo

0 Kudos
Reply

1,519 Views
intractablesubt
Contributor III

I had not seen those. Thanks!

0 Kudos
Reply

1,519 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello giac,

Does the demo of " sdhc_sdcard" in "C:\Freescale\KSDK_1.0.0\demos"  can meet you ?

Hope it helps

Alice

0 Kudos
Reply

1,519 Views
giacomopetrini
Contributor IV

Hi,

unfortunately the demo sdhc_sdcard does not use fatfs, so it has no use for me.

Best regards

Giacomo

0 Kudos
Reply