Debugger disconnects after code download

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugger disconnects after code download

跳至解决方案
15,700 次查看
bitjockey
Contributor II

Hello,

 

I am using a KE06 freedom board an was compiling, downloading, and debugging with no problems. Yesterday when I had compiled and downloading software the PE debugger disconnects and does not end up at the main() breakpoint. I have taken a snapshot of the debug screen when this happens. I see that the error is "source not found 0x1ba8", if I look in the map file that address corresponds to thumb startup code (see snippet below), why would it not be able to find that? Isn't that automatically generated? I am using processor expert to generate the low level stuff....

 

.text.__thumb_startup

                0x00001ba8       0x48 ./Project_Settings/Startup_Code/startup.o

                0x00001ba8                __thumb_startup

 

Any help would be appreciated.

Thanks,

Brian

标签 (1)
1 解答
12,701 次查看
davidsherman
Senior Contributor I

Okay!  KDS does seem to be temperamental.  On a whim, I tried figuring out this error with the source file was about.  So, I copied it off, deleted it from the project, added a new source file with the same name, then copied over the old one.  Now, not only is the source file error message gone, but I can re-enable all the source lines and the debugger runs.  I can even make that pointer to the ROM structure again, and it's still good.  Crazy...  I'd log more bug reports about the strange things I've seen in KDS, like occasionally not being able to build at all because it says it can't write to temp files, but these things are so random I can't reproduce them.  Thanks for your assistance, Erich.  My apologies to the OP as well, I didn't mean to hijack your thread :smileysilly:.

在原帖中查看解决方案

0 项奖励
回复
30 回复数
3,518 次查看
davidsherman
Senior Contributor I

Thanks Erich, I tried using the "clean" option and rebuilding, but it had no effect on the issue I was seeing.  The only thing I'm leaning toward is it having files edited outside of KDS.  I had the map file and the suspect source file open in an outside text editor, and I wonder if that was causing problems.

0 项奖励
回复
3,518 次查看
BlackNight
NXP Employee
NXP Employee

Having the source file open should not matter at all. And if the file has been touched outside the IDE, Eclipse is pretty good to detect that. Where I had a problem in the past was that GDB was running as a zombie process (not terminated), and it kept the .elf file open. Rebuilding the files did not help, and the linker complained about the .elf file not accessible. Killing the gdb excecuable from the Windows task manager solved that problem :-)

0 项奖励
回复
3,518 次查看
DavidLundquist
Contributor I

Interestingly I've just run into the same exact issue.  My GDB Log is identical to what was posted earlier by David Sherman.  Using the PE Micro Multilink Universal. 

I had been making some very minor incremental code changes and this problem popped up.  Backing them out doesn't seem to get me back to a working config.

Confirmed that none of my GPIO configs are stepping on the SWD lines.  NMI is not enabled.

Anyone else seeing this have any advice beyond what David Sherman did to "reload" his

0 项奖励
回复
3,518 次查看
roreith
Contributor I

I think I just cured the same problem by doing Remove All breakpoints.

I haven't had a chance to reproduce the issue and test this fix, but I had already tried fiddling with the USB connection and P&E USB Multilink / OSBDM/OSJTAG setup in the debug configuration, restarting Kinetis Design Studio, restarting the PC, etc.

I have had gdb (arm-none-eabi-gdb.exe) keep running in the background sometimes (if this happens, perhaps try using the red square "Terminate" button on the console window), but that is not what was causing this disconnect-after-download issue. It makes sense to me that a badly-placed breakpoint could upset the CPU following reset. Hopefully some other users can shed more light on this?

3,513 次查看
robcasey
Contributor I

Another vote from me Ro Reith - Same problem and same solution.

In my instance, I am using KDS 2.0.0 with TWR-KV10Z32 connected via the OpenSDA Embedded Debug - USB Port.

0 项奖励
回复
3,518 次查看
claybarclay
Contributor II

Ro Reith, You are my hero,  I did everything for the same problem (hours lost) then found your post about removing all break points and bang!  I am off an running again!

thanks much:smileyhappy:

BTW I am using KDS 1.1.1 on a K60DN512Z no OS

0 项奖励
回复
3,518 次查看
nickheppermann
Contributor I

I too have just seen similar behavior to Ro Reith and Clay Barclay.  I am using PE Micro USB Universal Multilink to debug my firmware and it seems to work for a few hours and then just stop working, failing in the same manner as the original poster described.  Hopefully this is the only fix that is needed.

0 项奖励
回复
3,518 次查看
BlackNight
NXP Employee
NXP Employee

Does it happen as well if you download a simple/new project wizard created project?

Erich

0 项奖励
回复
3,518 次查看
BlackNight
NXP Employee
NXP Employee

could you post your console logs of the debugger?

What about using another board?

Power supply?

USB cable to the probe?

I had once a half-dead debug cable which had kind of same symptoms, so do you have a spare one?

Erich

0 项奖励
回复
3,518 次查看
bitjockey
Contributor II

Erich,

Thanks for the quick reply, I didn't reconfigure any pins. I took your advice and entered the _thumb_startup in my debug startup menu. Inadvertently forgot the second underscore at the beginning and when I started the debugger it operated as normal breakpointing at 'main'. Went back in and entered main in my debug startup breakpoint and it still works?!?! I looked to me that the debugger was not pointing to where the _thumb_startup code should be, or the startup code did not compile correctly or output into the elf file correctly....I will keep an eye on it, if it happens again I will try to isolate what is going on.

Brian

0 项奖励
回复