Debug and run programs in FRDM-KL82Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debug and run programs in FRDM-KL82Z

跳至解决方案
2,870 次查看
angelgz
Contributor II

Hi,

I am having trouble trying to debug and run a program in my FRDM-KL82Z. I have followed all the steps in the guide online:

 - Installed the SDK 2.0 with the wizard for the kinetis design studio.

 - I have the jlink bootloader loaded in the board.

- I import one of the examples of the SDK ( ../boards\frdmkl82z\demo_apps\bubble\kds )

- I build the project with 0 errors:

Building target: bubble_frdmkl82z.elf
Invoking: Cross ARM C++ Linker
arm-none-eabi-g++ -mcpu=cortex-m0plus -mthumb -mfloat-abi=soft -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -fno-common -ffreestanding -fno-builtin -Wall -g -T ../settings/MKL82Z128xxx7_flash.ld -Xlinker --gc-sections -Wl,-Map,"bubble_frdmkl82z.map" --specs=nano.specs -mapcs -Xlinker -static -Xlinker -z -Xlinker muldefs -o "bubble_frdmkl82z.elf" -Xlinker --start-group ./utilities/fsl_debug_console.o ./startup/startup_MKL82Z7.o ./startup/system_MKL82Z7.o ./source/bubble.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_flash.o ./drivers/fsl_gpio.o ./drivers/fsl_i2c.o ./drivers/fsl_lpuart.o ./drivers/fsl_smc.o ./drivers/fsl_tpm.o ./board/board.o ./board/clock_config.o ./board/pin_mux.o ./accel/fsl_fxos.o -lm -lg -lgcc -lnosys -Xlinker --end-group
Finished building target: bubble_frdmkl82z.elf

12:59:37 Build Finished (took 1s.532ms)

- I launch the debug with the following configuration.

pastedImage_2.png

And when the debug perpective open, the program is already running ( I dont have to press startand the program is supposed to start as halted) 

pastedImage_3.png

If I pause the program is always in this state:

pastedImage_4.png

Any ideas why?

Thank you,

Angel

标记 (1)
0 项奖励
回复
1 解答
2,630 次查看
angelgz
Contributor II

Hi! 

I have just found a solution. I checked the breakpoint at main and it was already set, I tried switching workspace but the debugger keeps faulting. The solution was to start the debugging: It will start in the same status as stated in the first post (with a hard fault) but, if I press the reset button while in that state, the debug start working as normal. I show it in pictures for anyone that has my same problem.

Start the debugger, here the program seems to be working but it is not. If you pause it, you will see it is in the Hardfault ISR.

pastedImage_1.png

Press the reset button of the FRDM-KL82Z: The debugger get into the correct status :smileygrin: :smileygrin: :smileygrin: :smileygrin:

pastedImage_2.png

Press play and enjoy :smileyhappy:

I hope this help some other folks around there :smileyhappy:

See you and thank you very much!

Angel

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,631 次查看
angelgz
Contributor II

Hi! 

I have just found a solution. I checked the breakpoint at main and it was already set, I tried switching workspace but the debugger keeps faulting. The solution was to start the debugging: It will start in the same status as stated in the first post (with a hard fault) but, if I press the reset button while in that state, the debug start working as normal. I show it in pictures for anyone that has my same problem.

Start the debugger, here the program seems to be working but it is not. If you pause it, you will see it is in the Hardfault ISR.

pastedImage_1.png

Press the reset button of the FRDM-KL82Z: The debugger get into the correct status :smileygrin: :smileygrin: :smileygrin: :smileygrin:

pastedImage_2.png

Press play and enjoy :smileyhappy:

I hope this help some other folks around there :smileyhappy:

See you and thank you very much!

Angel

0 项奖励
回复
2,630 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Angel,

- Have you set breakpoint at main :

pastedImage_1.png

- Please try to switch another new workspace to have a try, or test another project.

pastedImage_2.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,630 次查看
angelgz
Contributor II

Ok, I will try this afternoon

However, its weird because yesterday I get it working for a few times. Its like it depends on what I flash before. I was trying using KSDK 1.3, then 2.2, different project settings... The same project sometime works, sometimes it doesn't... Maybe its a problem with the Jlink software? If I flash the same code and run it without debug it works, and I read that in some processors the j-link forget to turn on some clock or something like that... Also this would explain why sometimes it works (if some register is not clear on debug and was previously set correctly may result in the debug working...) I am just throwing some ideas...

Now I am just uploading the code without debug and using printf to debug (old-school debugging).

0 项奖励
回复
2,630 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Angel,

- If you worry about the project flashed impacting the new project, please

erase the flash use j-link commander (can download at to https://www.segger.com  ), and

see the attached video created by my colleague .

- Yes, if download many times, it maybe occur some problem, you can also delete the .metadata folder under

workspace :

pastedImage_1.png

BR

Alice

0 项奖励
回复