Customer discovered several issues with KDS 3.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Customer discovered several issues with KDS 3.0

823 次查看
jwu
Contributor I

1. The PinSettings PE component affects PWM output with uncertainty.

I set pin PTB5 as PWM output in FTM2. But, I didn’t get PWM output initially. When I
checked the FTM tab in Pin1Settings module, I clicked the channel 5 pin
selection for PTB5, which was already there. I then regenerated PE and I got
PWM output. This didn’t happen to PMW pin only. It happened to GPIO pins as
well.

My question is what’s the functionality of PinSettings generated module? Why do I have to
confirm pin selections when they appear to be selected already?


2. I initialized one ADC channels in ADC0 module. But, PinSettings module shows 5
channels. I have no option to change the pin selections in PinSettings module.

 

My question is: how PinSettings module affect ADC channel selection?

 

3. I selected 4 ADC channels from pin PTB0, PTA6, PTA1, and PTA0 in A/D channel
list. And, I created a “Static sample groups” that including samples of the 4
ADC channels. But, I got the channel readings that do not match physical
voltage on these pins.

 

My question is: how to make the “Static sample groups” working?

 

4. Casting from an address not 16-bit aligned in physical memory, causes MCU exception.

For example

Struct

{


uint8 b0;  uint8 b1;  uint8 b2;  uint8 b3;  uint8 b4;
uint8 b5;  uint8 b6;  uint8 b7;

}
FooStruct;

 

FooStruct
zData;

uint16*
pu16Ptr;

 

  pu16Ptr = (uint16*)zData.b3;   
<<----- this causes MCU exception.

 

My question is: It is very hard to patch source code to dodge this issue. Is it possible
changed some compiler setting to avoid this issue?

 

5. . I could not see the peripheral registers in KDS 3.0.0 when I debug software. How can I see them?

 

Thanks,
John

标签 (1)
0 项奖励
回复
1 回复

728 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello John,

1. After you configure the PinSettings PE component , click generate processor expert code ,

pastedImage_0.png

you can find the configure code in the cup.c file.

pastedImage_1.png

And about the PWM , you can also use the PWM_LDD component :

pastedImage_2.png

2. About change ADC channel pins , please in the ADC component :

pastedImage_3.png

3. Could you please show the code or configure about how do you

created a “Static sample groups” that including samples of the 4

ADC channels ?

4 . Which chip do you use ?

5. You can check the registers here :

pastedImage_4.png

pastedImage_5.png

pastedImage_6.png


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复