Creating a New MQX RTOS for KSDK Project in KDS for the MK60DX256Zxxx10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Creating a New MQX RTOS for KSDK Project in KDS for the MK60DX256Zxxx10

跳至解决方案
1,004 次查看
nickerb
Contributor I

As per the title, I am following the guide "Creating a New MQX RTOS for KSDK Project in KDS".  We are using the MK60DX256Zxxx10 processor and our own custom PCB.  When I go to make the project, however, I get hung up on step 2.4, as Kinetis SDK is greyed out.  I have downloaded and installed the latest KDS and KSDK, as well as gone through the salient upgrades from the KDS eclipse client.  Are the K60 processors not supported by the latest KSDK version?  Must I do something else before I can continue the tutorial?

 

Thanks.

标签 (1)
0 项奖励
回复
1 解答
635 次查看
DavidS
NXP Employee
NXP Employee

Hi Nick,

Hmmm.

Are you shure you did the following two steps?

1.3 See chapter 5.2 Install Eclipse update of ‘Getting Started with Kinetis SDK (KSDK)’ document located in KSDK installation path: C:\Freescale\KSDK_1.1.0\doc\Getting Started with Kinetis SDK (KSDK).pdf

1.4 Verify that ‘KSDK_PATH’ environment variable is set correctly. See ‘Appendix B’ in this document

I've always tossed in a re-boot after doing this.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
3 回复数
635 次查看
DavidS
NXP Employee
NXP Employee

Hi Nick,

Try using same part/device number without the "Z" then the Kinetis SDK is not greyed out.

"Z" usually indicates first revision of silicon.  When I look online I only see device part numbers without the "Z".

Regards,

David

0 项奖励
回复
635 次查看
nickerb
Contributor I

Hi David,

Sadly, every MK60D, MK60F and MK61F processor listed have KSDK greyed out.

0 项奖励
回复
636 次查看
DavidS
NXP Employee
NXP Employee

Hi Nick,

Hmmm.

Are you shure you did the following two steps?

1.3 See chapter 5.2 Install Eclipse update of ‘Getting Started with Kinetis SDK (KSDK)’ document located in KSDK installation path: C:\Freescale\KSDK_1.1.0\doc\Getting Started with Kinetis SDK (KSDK).pdf

1.4 Verify that ‘KSDK_PATH’ environment variable is set correctly. See ‘Appendix B’ in this document

I've always tossed in a re-boot after doing this.

Regards,

David

0 项奖励
回复