Hi,
We are working on KL03 with KDS3.1.0 + PE,
As I can see in datasheet there are power modes available as Normal Run, Normal Wait, Normal Stop, VLPR, VLPW etc..
Please guide me how can I change the power modes of the KL03 in programming using KDS IDE,
Or is there document/ tutorial for changing the power modes using KDS programming?
Regards,
Idris
已解决! 转到解答。
Hello Idris,
The attachment is a demo on CodeWarrior +PE , it is the same with KDS.
You can open it on CW, then create one new project on KDS, refer to the demo to develop.
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Idris,
The attachment is a demo on CodeWarrior +PE , it is the same with KDS.
You can open it on CW, then create one new project on KDS, refer to the demo to develop.
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------