Changing Vrefh of ADC in KL03

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changing Vrefh of ADC in KL03

Jump to solution
1,050 Views
syedidris
Contributor III

Hi,

I am working on Kinetis KL03 with KDS 3.0.0. when I am connecting current senser ACS 712 with ADC (12bit resolution), ADC is taking 3v as Vrefh.

I want to know that is it possible to give externally 5v as a vrefh to ADC of KL03 ?

Labels (1)
Tags (1)
1 Solution
893 Views
DavidS
NXP Employee
NXP Employee

Max is VDDA which is same as max VDD of 3.6VDC.

Use voltage divider to reduce 5V to VDD.

Regards,

David

PS information in device datasheet

Sent from David Seymour's iPhone 6

View solution in original post

1 Reply
894 Views
DavidS
NXP Employee
NXP Employee

Max is VDDA which is same as max VDD of 3.6VDC.

Use voltage divider to reduce 5V to VDD.

Regards,

David

PS information in device datasheet

Sent from David Seymour's iPhone 6