Cant get my Cyclone programming FRDM-KL27

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cant get my Cyclone programming FRDM-KL27

ソリューションへジャンプ
1,664件の閲覧回数
carlnormansuret
Contributor V

Hi Guys,

 

I have a service request with PE Micro, but no response in 24 hours, im in a panic, i need to get this working ASAP. Maybe someone can share a solution.

 

Attached is the document i made with pictures and explanation. After 20 years of doing this, its honestly a little to hard for a simple job.

 

Read the document for details, but a quick summary; Basically I learnt you cant make your own adapter for the Cyclone MAX for SWD programming as they "do something special" on their external adapter to enable SWD programming mode. My understanding (from endless googling) is all it does is short Pin 3 and 10 on Port B of the cyclone (which translates to something on Port E being shorted). I have done this and nothing happens. I have the hello world basic FRDM KL27 application, works perfectly through openSDA, nothing through cyclone, reset is low, nothing changes.

ラベル(1)
1 解決策
1,510件の閲覧回数
carlnormansuret
Contributor V

For anyone else that has this problem, there are some serious issues with the cyclone documentation!

This is the correct diagram for Port E:

pastedImage_1.png

You have to short out (so its easy) port B pins 3 and 10 to enable SWD mode

My problem was there is two diagrams, and hte flash configuration tool tells you to use the wrong one.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,511件の閲覧回数
carlnormansuret
Contributor V

For anyone else that has this problem, there are some serious issues with the cyclone documentation!

This is the correct diagram for Port E:

pastedImage_1.png

You have to short out (so its easy) port B pins 3 and 10 to enable SWD mode

My problem was there is two diagrams, and hte flash configuration tool tells you to use the wrong one.

0 件の賞賛
返信
1,510件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Carl,

Thanks for your sharing .

BR

Alice