I compiled my code on KDS for FRDM-K64F. I got the elf file but I am not getting the output on tera term. I have set the baud rate=115200, data bits=8, no parity bits and 1 stop bit. Also the size of the .elf is 1.98mb. I would appreciate if someone could help me
解決済! 解決策の投稿を見る。
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Kiran,
If you want use the printf function of KSDK , the name is "debug_printf", "debug_scanf":
please be careful that in the function of "debug_scanf" , the IO_MAXLINE is 20
you can refer to your demand to change it .
I also attached my project .
BR
Alice
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Alice,
I am working on a frequency generator project. 
I wanted to direct you to this link. Please let me know if you can help?
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Kiran,
My colleague have checked your question , he will reply to you .
Have a nice day !
Alice
Thank you Alice. The solution works :smileyhappy:
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Kiran,
- Please be sue which UART you used , check the SCH and your code .
- What about your project ? Bare board project ? PE project ? KSDK ? You'd better send it to me .
- And you can also first find one demo project to test .
Hope it helps
Alice
Hi Alice,
I missed to add some files and paths. 
Now, I have "MK64F12/include/MK64F12.h: No such file or directory" error.
Please let me know if you have any solution?
Thank you,
Kiran
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Kiran,
Please tell me the version of KDS, and also the KSDK version , KSDK1.2 OR ksdk 1.3 ?
Then please send file you changed , the method is click the "Actions" button , then click "Edit" ,
then you can find the "attach"
Alice
Hello Alice,
I am using KDS Version: 3.2.0 and KSDK 1.3.
Also, now I am getting new issues with the debug
I build the project and after debugging I get the following:
No source available for "(gdb[1].proc[42000].threadGroup[i1],gdb[1].proc[42000].OSthread[1]).thread[1].frame[0]"
No source available for "0x3848"
No source available for "0x2592"
The address keeps changing. I also get the following warning on the console:
Warning: the current language does not match this frame.
Temporary breakpoint 2, main () at ../Sources/main.c:65
65 PE_low_level_init();
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Kiran,
Are you sure this main.c file you send to me is changed under the KSDK demo ?
I think no , for the header files you include in the main.c file are some header file the PE
generate . So i have some confused.
If you want use the KSDK+PE create one project , please create one new project.
And you can also describe your project in detail , then we can find the problem sooner.
BR
Alice
Hi Alice,
I was confused with the use of PE. I tried a simple "Hello World" program with PE, it worked. I cannot make scanf work on tera term. My project is to design a frequency generator(pattern generator with 1 and 0 bits) for crank and cam. Is it possible to run my code with KSDK+PE. I have attached my original C code below.
Hello Alice,
Thank you for replying. It is a Kinetis SDK 1.x project.
I tried to run the demo code for "Hello World!" and it worked fine.
I copied 750 lines of my C code in main.c file. I was wondering if it is the size.
How can I send you the code? Is there a way to send a file?
I'm new to this and would appreciate any help.