Hello Juan,
We need first build the platform library project in KDS IDE, the platform library is
required by the demo. So your step is is import the lib , build it , the path is you said :
(in<install_dir>/lib/ksdk_platform_lib/kds/KL46Z4)
Then you can import example : KSDK_1.2.0\examples\frdmkl46z\demo_apps or
SDK_1.2.0\examples\frdmkl46z\driver_examples .
About the detail steps please refer to "Getting Started with Kinetis SDK (KSDK) v.1.3.pdf
" (under KSDK_1.2.0\doc) .
If you want use the KSDK1.x, I recommend you use the latest version KSDK1.3.
And also there is KSDKv2.x (This version without Processor Expert) .
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------