Can't start debugger using J-LINK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't start debugger using J-LINK

2,127 Views
predragvidic
Contributor I

When try to debug my project, which bilds without any problem, (Segger J-LINK) the KDS 3.2.0 replies: 'Launching my_project_name debug' has encountered a problem. Program file does not exist.

Also debugger continues to try to start and is continuously on 62%

I have followed the steps from the KDS user manual

3 Replies

1,919 Views
BlackNight
NXP Employee
NXP Employee

Does that file you want to debug exist in the debug folder? The message indicates that it does not exist. Can you check if it exists on disk *and* in the project 'debug' folder? If it exists on disk, you might need to do a Refresh/F5 on the debug folder inside the Project view.

I hope this helps,

Erich

1,919 Views
predragvidic
Contributor I

Thanks a lot. Helped.

0 Kudos
Reply

1,919 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Predrag

I suggest you move this question to KDS space

https://community.nxp.com/community/mcuxpresso/kinetis-design-studio 

There are NXP KDS expert monitoring KDS space.

Jennie Zhang

0 Kudos
Reply