Can't start J-Link GDB server on TWR-K70F120M, KDS 3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't start J-Link GDB server on TWR-K70F120M, KDS 3.0

Jump to solution
507 Views
kirkdavis
Contributor I

I am trying to use KDS 3.0 with a TWR-K70F120M and TWR-SER tower system.  I can't get the J-Link GDB server started.  I always get the "No emulators connected via USB" error.  I have two USB connections on the tower system, and they show up in the Windows 7 Device Mgr as OSBDM/OSJTAG - Debug Port (http://www.pemicro.com/osbdm) and OSBDM/OSJTAG - CDC Serial Port (http://www.pemicro.com/osbdm, http://www.pemircro.com/opensda).  I have worked through the user, quickstart, and troubleshooting guides, checked the jumpers, ran the P&E Firmware Updater utility, etc., but always get the same results.  Any ideas?

Labels (1)
0 Kudos
1 Solution
373 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kirk,

If your board has the P&E OSJTAG firmware the you need to select the "PEMicro Interface Debugging" connection:

pastedImage_0.png

And make sure your board is detected:

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer
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
374 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kirk,

If your board has the P&E OSJTAG firmware the you need to select the "PEMicro Interface Debugging" connection:

pastedImage_0.png

And make sure your board is detected:

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos