A project based on K20 is requested to move on to K60. I tried to run the firmware wroten for K60 on a K20 hardware, and it seems OK. So I wonder if a K20 firmware can run directly on K60 without recompile.
Or, if not, what should I do to port a K20 firmware to K60? Changing the MCU and pin names (same pin has different names between K20 and K60) in ProcesserExpert would be enough?
Thank you.
Hello ,
Please refer to the reference manual to compare the two chips ,
especially the modules that your project used.
For example , UART, SPI, check the memory address, pins and other related things.
Also check the flash size .
BR
Alice