Can firmware developped for K20 rum on K60?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can firmware developped for K20 rum on K60?

742 Views
huangda1982
Contributor I

A project based on K20 is requested to move on to K60. I tried to run the firmware wroten for K60 on a K20 hardware, and it seems OK. So I wonder if a K20 firmware can run directly on K60 without recompile.

Or, if not, what should I do to port a K20 firmware to K60? Changing the MCU and pin names (same pin has different names between K20 and K60) in ProcesserExpert would be enough?

Thank you.

0 Kudos
Reply
1 Reply

635 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Please refer to the reference manual to compare the two chips ,

especially the modules that  your project used. 

For example , UART, SPI, check the memory address, pins and other related things.

Also check the flash size .

BR

Alice

0 Kudos
Reply