Can KDS be used to flash application at particular memory address?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can KDS be used to flash application at particular memory address?

1,429件の閲覧回数
tonysonney
Contributor I

Hi

     I know KDS can be used to flash binaries from address 0x0. But can it be used to flash the binary to another address, say from 0x100? I am using TWR-K65180M.

Many Thanks,

Tony

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,226件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tony,

Refer to my test , in kds 3.0 , it can not flash the binary file , could you tell me how do you

flash the binary file use KDS, thank you very much !

BR

Alice

0 件の賞賛
返信

1,226件の閲覧回数
tonysonney
Contributor I

Hi Alice,

          My board is connected to the PC over USB. With the Segger firmware loaded, KDS detects it as a jlink device. Then using KDS I can compile applications and then either hit F11 or use Menu options Run->Run. This should load the board with the built binary and run.

Cheers,

Tony

0 件の賞賛
返信

1,226件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tony,

On the debug configuration, are you sure you select the ".bin " file :

pastedImage_0.png

BR

Alice

0 件の賞賛
返信