Bug in KDS when using CMSIS in C++ - Was: Kinetis Design Studio and C++

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bug in KDS when using CMSIS in C++ - Was: Kinetis Design Studio and C++

跳至解决方案
1,511 次查看
Masmiseim
Senior Contributor I

Hello,

 

Until know I was working with Rowley Crossworks for Embedded Development and I’m quite happy with it. But I wanted to give KDS (v3.0) a try.

I created a simple Project without using Processor-Expert or KSDK. I renamed the automatically created main.c file to main.cpp and added some includes to the CMSIS files.  You can find the resulting main.cpp File as an attachment.

 

Compiling this leads to an error in the CMSIS include File:

../Includes/core_cm4.h:1787:1: error: expected declaration before '}' token

 

It should definitely compile. Has KDS some problems with C++?

 

Thanks and regards

 

Markus

Original Attachment has been moved to: main.cpp.zip

标签 (1)
1 解答
1,236 次查看
Masmiseim
Senior Contributor I

Hello,

OK I fixed it on my own. It is not a C++ problem.

The CMSIS-Headerfiles delivered with KDS3.0 are rather old and seems to have some bugs which lead to the described Errors, but only when compiled as C++.

I replaced the CMSIS Files with the current Version. Now it is compiling without problems.

Regards

Markus

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,237 次查看
Masmiseim
Senior Contributor I

Hello,

OK I fixed it on my own. It is not a C++ problem.

The CMSIS-Headerfiles delivered with KDS3.0 are rather old and seems to have some bugs which lead to the described Errors, but only when compiled as C++.

I replaced the CMSIS Files with the current Version. Now it is compiling without problems.

Regards

Markus

0 项奖励
回复
1,236 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Markus.

please refer Erich blog for C++ with Kinetis Design Studio:

C++ with Kinetis Design Studio | MCU on Eclipse

this article may help you.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,236 次查看
Masmiseim
Senior Contributor I

Hello Zhang Jun,

thanks for your feedback. I know Erich’s blog, and I like it very much.

Erich says in his blog:

“Bare Projects with C++

If using C++ with a bare project type, then everything is setup correctly. You only need to make sure that header files included for C++ files are listed in the compiler include path settings:”

This means I shouldn’t have any problems, but I do.

The only things I did was renaming main.c to main.cpp and added the include instruction

#include <core_cm4.h>

#include <core_cmInstr.h>

#include <core_cmFunc.h>

This Blog is abound Version 1.1.1. Maybe something changed to the current Version?

Thanks and regards

Markus

0 项奖励
回复