Bug: KDS fails to start debug with "Error in final launch sequence"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug: KDS fails to start debug with "Error in final launch sequence"

933 Views
davenadler
Senior Contributor I

K64F Freedom board, latest KDS (all updates as of last week).
Debug was working OK and suddenly I get the following error when trying to launch debugger:
170487_170487.PNGKDS OpenOCD fails to start debug.PNG

If I power-cycle the board I can drag-and-drop a "hello world blinky light" application into the mbed drive and it works, so the board seems to be OK. There are no zombie debug processes (the problem happens every time on clean start of KDS and board).

 

Anybody have any idea what's going on?

Thanks,
Best Regards, Dave

 

PS: Alice, please do not suggest I re-install Windows or other silliness.

PPS: The following users have reported related problems with no problem resolution:

https://community.nxp.com/message/832787

https://community.nxp.com/message/832828

https://community.nxp.com/message/665363

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

798 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Dave,

is this the same issue as https://community.nxp.com/thread/439738 ?

if yes please refer above thread of my response.

Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply