Bootloader for Kinetis K64 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader for Kinetis K64 MCU

Jump to solution
3,670 Views
小勇邹
Contributor II

I try to develop the bootloader via usart and enternet for Kinetis K64 MCU. Is there any source code example?

Labels (1)
0 Kudos
Reply
1 Solution
2,410 Views
mjbcswitzerland
Specialist V

Hi

See https://community.freescale.com/message/370223#370223

Supports K64 for UART, USB, Ethernet, SD-card bootloading. Web server based loading occupies about 18k of space built with GCC.

Regards

Mark

http://www.utasker.com/kinetis.html

View solution in original post

0 Kudos
Reply
2 Replies
2,411 Views
mjbcswitzerland
Specialist V

Hi

See https://community.freescale.com/message/370223#370223

Supports K64 for UART, USB, Ethernet, SD-card bootloading. Web server based loading occupies about 18k of space built with GCC.

Regards

Mark

http://www.utasker.com/kinetis.html

0 Kudos
Reply
2,410 Views
DavidBLit
Contributor II

You could try porting Emcraft's U-Boot here, but be aware it's a very old U-Boot and its Kinetis support is pretty thin and anemic.

I think the biggest bite would be the MCG differences between the K70 and the K64.

Maybe you could be a hero and fix all that...  :smileywink: