I used to use it all the time FRDM_K64F (getting a jump on my firmware), then started using P&E, which works great on FRDM and also on my hardware.
Recently went back to the FRDM because I left the P&E Multilink Universal at home, and I make new OpenOCD (is this = OpenSDA?) anyway, the -f Kinetis.cfg is there, it goes through the motions and then crashes.I can (after fiddling with J8/J11/J25) can use the P&E on this board...
Am I missing something obvious here?
A flash of red on the console, then then the GNU License info...
"GNU gdb (GNU Tools for ARM Embedded Processors) 7.6.0.20140731-cvs...."
On the debug screen the only active button is "Terminate".
Using P&E for now. This FRDM_K64F board has not changed since I got it working months ago.
I don't remember seeing an errata on this, and I doubt you would have broken the FRDM OpenSDA with KDS 3.0... lolz
EDIT: Note I have a stock P&E - I don't have the OpenSDA firmware loaded onto it on purpose.