I keep getting this message when I debug:
I have checked it against configurations that I had been using in KDS 2.0 and they are identical. I even get this when debugging the demo applications. How do I get details about the specific errors, and how would I then fix them?
If I proceed, everything seems to run normally, and I can still use the debugger.
已解决! 转到解答。
FWIW, I've observed this on occasion in KDS_v3 as well (on Mac OSX 10.12.6 / Sierra). Quitting and restarting KDS has fixed it.
Now that I think about it, I saw this error dialog after I renamed some files out from under the project manager (e.g. "git rm xxx", etc), which probably confused it.
The usual cause of this message are wrong paths/settings in the project. See
"Errors exist in the active configuration..." Eclipse Dialog when Debugging - Stack Overflow
I hope this helps,
Erich
I could not find a wrong path setting in the project.
Deleting the launch configuration did not fix the issue permanently. The first debug session succeeded without this message, subsequent debug sessions prompted this message.
Deleting the current build folder (i.e., "Debug") resolved the issue for me permanently in one project. However, for a second project that "fix" didn't work.
Hi Dave,
For there are many MQX demo , for example MQX 4.0 MQX 4.1 MQX 4.2 , OR KSDK-MQX, ..
So please tell me the detail path of the demo in you PC. Take the hello demo for example, you can show like this to tell me :
"....Freescale\KSDK_1.2.0\rtos\mqx\mqx\examples\hello\build "
Thank !
Alice