I keep getting this message when I debug:
I have checked it against configurations that I had been using in KDS 2.0 and they are identical. I even get this when debugging the demo applications. How do I get details about the specific errors, and how would I then fix them?
If I proceed, everything seems to run normally, and I can still use the debugger.
解決済! 解決策の投稿を見る。
Alice, I'm not sure what happened, but I recently rebooted my computer, and now I don't get this problem anymore. :smileyhappy: Weird!
FWIW, I've observed this on occasion in KDS_v3 as well (on Mac OSX 10.12.6 / Sierra). Quitting and restarting KDS has fixed it.
Now that I think about it, I saw this error dialog after I renamed some files out from under the project manager (e.g. "git rm xxx", etc), which probably confused it.
I have a same problem now,but i can't bug if i proceed, there two item of error.
That seems like a bug.
I'm going to give up KDS and try ARM Keil.
The usual cause of this message are wrong paths/settings in the project. See
"Errors exist in the active configuration..." Eclipse Dialog when Debugging - Stack Overflow
I hope this helps,
Erich
I could not find a wrong path setting in the project.
Deleting the launch configuration did not fix the issue permanently. The first debug session succeeded without this message, subsequent debug sessions prompted this message.
Deleting the current build folder (i.e., "Debug") resolved the issue for me permanently in one project. However, for a second project that "fix" didn't work.
Hello ,
""I even get this when debugging the demo applications." Please tell me which demo , I will test on my side , thank !
BR
Alice
It's the one shown in my screenshot. :smileyhappy: lwip_tcpecho_demo_mqx_frdmk64f
Hi Dave,
For there are many MQX demo , for example MQX 4.0 MQX 4.1 MQX 4.2 , OR KSDK-MQX, ..
So please tell me the detail path of the demo in you PC. Take the hello demo for example, you can show like this to tell me :
"....Freescale\KSDK_1.2.0\rtos\mqx\mqx\examples\hello\build "
Thank !
Alice
Ah, I understand. :smileyhappy: Here you go: C:\Freescale\KSDK_1.2.0\examples\frdmk64f\demo_apps\lwip\lwip_tcpecho_demo\tcpecho_rtos\tcpecho_mqx\kds
Hi Dave,
I have test it , on my side , there is no this reminder .
And have you compile the MQX lib before you build the demo .
BR
Alice
Alice, I'm not sure what happened, but I recently rebooted my computer, and now I don't get this problem anymore. :smileyhappy: Weird!