I'm working with KDS 3.2.0, and want to create a project using the Kinetis K26 or K66. Howevere, they don't seem to be supported by PE, and I couldn't find any relevant update. Is there a way to add them to PE?
Thanks,
Eyal
Hello Eyal,
Yes, the PE doesn't support the two chips.
While the KSDKv1.3 also have PE, it support the two chips:
You can download it at here :
Software Development Kit for Kinetis MCUs|NXP
About the install into KDS , please refer to the "KDS_User_Guide" under : KDS_v3\doc\KDS_Users_Guide.pdf
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------