Using the FRDM-KL46 Board as a USB Keyboard in KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using the FRDM-KL46 Board as a USB Keyboard in KDS

Using the FRDM-KL46 Board as a USB Keyboard in KDS

USB Keyboard in KDS

 

Description:

 

A project made in KDS using the FRDM-MKL46Z256VLL4 board as a USB keyboard input.

A red LED will flash while not connected as a USB keyboard, and green LED will flash when it is.

Switch SW3 will type 'SW3 Pressed' and switch SW1 will type 'SW1 Pressed'

In Application.c is commented out example code for pressing print screen and control+alt+delete.

 

Sections of code taken from http://mcuoneclipse.com/2013/06/30/using-the-frdm-kl25z-as-usb-keyboard/

标签 (1)
附件
无评分
版本历史
最后更新:
‎07-03-2014 09:15 AM
更新人: