Uninstalling KDS: "Error opening installation log file."

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Uninstalling KDS: "Error opening installation log file."

Uninstalling KDS: "Error opening installation log file."

In case you are running into this error while trying to uninstall KDS on Windows (I had it with KDS V1.1.0, but it might apply to other versions too):

 

"Error opening installation log file. Verify that the specified log file location exists and is writeable."

14643_14643.pngpastedImage_0.png

 

After some googling, some installers (or uninstallers) can cause that error message. It seems that some files/folders are not accessible.

In my case I had it with installing KDS, and then wanted to uninstall it as I installed (in error) V1.1.0 (and not the latest V1.1.1).

I had not rebooted afterwards. But when I rebooted, the problem does go away.

 

So if you run into that problem: reboot your machine and try again. It worked for me.

 

Happy Uninstalling :-)

标签 (1)
无评分
版本历史
最后更新:
‎09-06-2014 07:01 AM
更新人: