Summary of FRDM-K22F debug interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Summary of FRDM-K22F debug interface

Summary of FRDM-K22F debug interface

NXP Freedom K22F is an ultra-low-cost development platform for Kinetis K22 MCUs. This board is already widely used among NXP customers.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-K22F

 

The FRDM-K22F platform features OpenSDAv2.1, which is a bit different as OpenSDAv2 on FRDM-K64F board.  The NXP open source hardware embedded serial and debug adapter running an open source bootloader. This circuit offers several options for serial communication, flash programming, and run-control debugging. User who works with KDS3.0 can choose Segger J-Link OpenSDA, P&E OpenSDA interface, or Mbed interface.  For each of the option, user need update debugger firmware first.  I will introduce each of them one by one.

 

All the related driver and firmware will be enclosed in this article as attachment.

 

Enjoy KDS + FRDM-K22F debugging. :-)

标签 (1)
附件
无评分
版本历史
最后更新:
‎03-14-2016 08:28 PM
更新人: