New Kinetis Design Studio V3.0.0 available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

New Kinetis Design Studio V3.0.0 available

New Kinetis Design Studio V3.0.0 available

Greetings,

the new Kinetis Design Studio V3.0.0 is available in the download section of the Freescale web:

http://www.freescale.com/kds

Kinetis Design Studio is free of charge and unlimited.

 

What's New

  • New Eclipse Luna 4.4 IDE
  • Added Mac OS X (10.10, "Yosemite") host operating system support with Segger J-Link.
  • Added CMSIS-SVD Peripheral Register viewer.
  • New 'Welcome' view
  • New GNU ARM Embedded (launchpad) toolchain, reducing memory footprint especially for small devices.
  • New upgrade/migration assistant to migrate projects to V3.0.0.
  • Updated and extended Segger and P&E debugging support: attach to running target, semihosting and advanced flash programming features.
  • New Processor Expert V3.0 with multiple repository support and simplified Kinetis SDK usage and ability to generate projects for IAR and Keil.
  • Updated New Project Wizard (NPW) for simpler project creation.
  • Updated GNU ARM Eclipse plugins, multiple tool chain configurations.
  • Aligned and optimized for Kinetis SDK v1.2
  • New Device Support: see attached release notes (Rev 1).

 

Additional Kinetis SDK Device Support

For full/additional device support:

  1. Download the Kinetis SDK v1.2 from Software Development Kit for Kinetis MCUs|Freescale
  2. Install the Kinetis SDK
  3. Add Kinetis SDK v1.2 to KDS: Use the menu Help > Install New Software and use C:\Freescale\KSDK_1.2.0\tools\eclipse_update\KSDK_1.2.0_Eclipse_Update (KSDK path on windows)

 

See https://community.freescale.com/docs/DOC-103698 for additional details, especially about porting KDS v2.0.0 projects to the GNU ARM Embedded (launchpad) tools.

 

Screenshots of new features

 

Mac OS X support:

22845_22845.pngpastedImage_1.png

 

New Workspace Welcome view:

22844_22844.pngpastedImage_0.png

 

Kinetis SDK selection in New Project Wizard:

22839_22839.pngpastedImage_0.png

 

Ability to generate Processor Expert (Microcontroller Driver Suite) external projects for IAR and Keil:

22840_22840.pngpastedImage_1.png

 

 

Eclipse Luna 4.4, e.g. Split Editor Views:

22846_22846.pngpastedImage_2.png

22847_22847.pngpastedImage_3.png

 

Processor Expert V3.0 and multiple component repositories:

22849_22849.pngpastedImage_0.png

22850_22850.pngpastedImage_1.png

 

Upgrade assistant to migrate projects from KDS V1.x/V2.0.0 to V3.0.0:

22851_22851.pngpastedImage_2.png

22852_22852.pngpastedImage_3.png

 

Multiple tool chain configurations:

22853_22853.pngpastedImage_4.png

 

Peripheral Register Viewer:

22855_22855.pngpastedImage_7.png

 

JTAG Daisy Chaining:

22856_22856.pngpastedImage_8.png

 

Advanced Flash Programming Options:

22858_22858.pngpastedImage_10.png

Attach to running target:

22857_22857.pngpastedImage_9.png

 

And finally, for the 'lovers of the dark side' :-): Eclipse Luna 'Dark' style:

22860_22860.pngpastedImage_1.png

 

Enjoy :-)

标签 (1)
附件
评论

Hi Erich,

Is the mac version already available?

In the KDS Download webpage there is no link for mac.

Thanks,

Alikds.png

Hi Ali,

I appologize for that, I have realized that too. Working with the web team to get that fixed. Will post a comment here when it is fixed.

Erich

Hi Ali,

the web download has been fixed, and the Mac OS X installer is available now.

Erich

Thanks Erich!

-Ali

Hi Erich,

The new KDS seems great so far! In the release notes for accessing the Register View, I think they meant to say:

"Window > Show View > Other > Debug" instead of Help > Show Views ...

-Angus

Hi Erich

kinetis M not support for kinetis dising 3.0

andres

Hi Andres,

yes, Kinetis M is not supported in KDS, because it is not supported in the Kinetis SDK (yet).

Erich

Hi Angus,

thanks for reporting this. This already has been fixed in the Rev1 version of the release notes (attached to this page). The installation comes with Rev0 which indeed has that error in it.

Erich

Hi Erich

1. Thanks for the MacOSX version!

2. What about support for Vybrid processors? For the standalone Driver Suite a Vybrid plugin exists, any plans to integrate into the latest KDS/SDK?

Vybrid.png

hi Erich

then that can be programmed Kinetis M,using process experts

thanks

Hi Robert,

there are currently no plans to have Vybrid added to Kinetis Design Studio.

Erich

Hi Erich, the Linux version .bin file cannot be installed.

./Kinetis\ Design\ Studio\ installer\ for\ Linux\ 64-bit\ DEB\ 3.0.0.bin

./Kinetis Design Studio installer for Linux 64-bit DEB 3.0.0.bin: line 1: syntax error near unexpected token `newline'

./Kinetis Design Studio installer for Linux 64-bit DEB 3.0.0.bin: line 1: `!<arch>'

mv ./Kinetis\ Design\ Studio\ installer\ for\ Linux\ 64-bit\ DEB\ 3.0.0.bin ./Kinetis\ Design\ Studio\ installer\ for\ Linux\ 64-bit\ DEB\ 3.0.0.deb

sudo dpkg -i ./Kinetis\ Design\ Studio\ installer\ for\ Linux\ 64-bit\ DEB\ 3.0.0.deb

Thanks. I wish Freescale had used .deb instead of .bin for Debian file.

Hi, If want to develop a commercial product can I do it with kinetis studio? Do I have to pay if I want to use it for the purpose?

Regards

Kinetis Design Studio can be used for commercial purposes, it has not limits except that it can be used for Freescale devices only.

Hi Erich,

My mac version is 10.11.1.

When I open KDS and select a workspace I can't click any buttons. It was stuck.

Hello,

are using El Capitan? If so, then it could be this problem (with solution):

KDS on OS X El Capitan (Beta)

I hope this helps,

Erich

It works. Thanks!

Hi Erich,

Using "Init_GPIO" it is possible to set pull-up or pull-down resistor in KDS V3.0.0?

I found examples using CodeWarrior!

Regards,

Arnaldo

Hi Arnaldo,

yes, this is possible with Processor Expert projects.

Erich

无评分
版本历史
最后更新:
‎05-06-2015 04:16 AM
更新人: