Generate aligned HEX and S-record data output with GNU in KDS 3.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Generate aligned HEX and S-record data output with GNU in KDS 3.2

Generate aligned HEX and S-record data output with GNU in KDS 3.2

Some customers have special requirements for the output data.  They need them to be aligned, especially when they are using the customized bootloader or Flash Programmer.  

 

However, the hex file generated in KDS3.2 is not aligned as the customer expected.

Below is extracted from the hex file generated in a KE06 project.  In this file, the data is not aligned at 16 bytes, and the size of each line is different.

154237_154237.pnghex_ori.png

 

The attached document shows generate aligned Hex and S-record file step by step.

标签 (1)
附件
无评分
版本历史
最后更新:
‎06-23-2016 05:15 PM
更新人: