Hi
need to use low power mode VLLS0
in the microcontroller documentation the Idd current specified for VLLS0 at 50°C max is 1µA
but when i used this mode the IDD is 50µA
who knows what to do
the code to enter VLLS0
NVIC_EnableIRQ(APP_WAKEUP_BUTTON_IRQ);
PORT_SetPinInterruptConfig(APP_WAKEUP_BUTTON_PORT, APP_WAKEUP_BUTTON_GPIO_PIN, APP_WAKEUP_BUTTON_IRQ_TYPE);
LLWU_SetExternalWakeupPinMode(LLWU, LLWU_WAKEUP_PIN_IDX, LLWU_WAKEUP_PIN_TYPE);
NVIC_EnableIRQ(LLWU_IRQn);
vlls_config.subMode = kSMC_StopSub0;
SMC_PreEnterStopModes();
SMC_SetPowerModeVlls(SMC, &vlls_config);
SMC_PostExitStopModes();
all the inputs are pullupdisable ...
many thanks for help
--