Peak Package Body Temperature of 32-bit Arm Cortex®-M3 microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Peak Package Body Temperature of 32-bit Arm Cortex®-M3 microcontroller

1,281 Views
SIGMAMARS
Contributor I
Hi Sir,
I have a trouble issue on soldering and need your professional advise . 
According to the date sheet of LPC1768FBD100K was shown Lead soldering PBT is 240℃ ,which is a
inconsistency with the label was shown PBT is 225℃。That means i can choose each one of them to process ?

 

企业微信截图_16195657544565.png企业微信截图_1619565810335.png

0 Kudos
Reply
1 Reply

1,260 Views
SIGMAMARS
Contributor I

No body answer this question ?

0 Kudos
Reply