KinetisFlashTool download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KinetisFlashTool download

1,249件の閲覧回数
sw1234
Contributor I

Hello.
I want to download the KinetisFlashTool.
But I don't know where to download it.
Can you tell me where it is?

sw1234_0-1704636993708.png


Thank you.

0 件の賞賛
返信
1 返信

1,098件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, pls refer to section Chapter 26 Kinetis ROM Bootloader in K32L3ARM.pdf, which can be  downloaded from the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

In other words, there is ROM bootloader, it is not necessary to load flashloader to the flash, you can use blhost to connect to the K32 directly.

You can use above tools to download application code in the ROM boot process.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信