I2C Slave Sleep Requirements

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Slave Sleep Requirements

Jump to solution
2,764 Views
jaredm
Contributor III

I am evaluating the K32L2B series microcontrollers for a new product.

The product requirements specify the microcontroller remain in sleep most of the time, but can be woken up by the I2C Slave peripheral. The I2C bus speed is always 400kbps.

When I2C is active, RUN mode is required to support 400kbps (per RM, VLPS only supports 100kbps).

When the system sleeping, VLPS is the preferred mode. According to the RM, I2C will support "static, address match wakeup" in VLPS mode.

Does "address match wakeup" work at 400kbps when in VLPS mode?

Tags (1)
0 Kudos
Reply
1 Solution
2,727 Views
jaredm
Contributor III

Testing has demonstrated that address match wakeup works at 400kbps in VLPS mode. The datasheet implies that the address match wakeup logic is independent of the normal slave receive logic. During address match wakeup the address bits are clocked in only using SCL, whereas normal slave receive uses the configured baud rate to sample and perform bit granularity clock stretching (if enabled).

 

View solution in original post

0 Kudos
Reply
1 Reply
2,728 Views
jaredm
Contributor III

Testing has demonstrated that address match wakeup works at 400kbps in VLPS mode. The datasheet implies that the address match wakeup logic is independent of the normal slave receive logic. During address match wakeup the address bits are clocked in only using SCL, whereas normal slave receive uses the configured baud rate to sample and perform bit granularity clock stretching (if enabled).

 

0 Kudos
Reply