How to Enable Secure Boot on K32L3A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Enable Secure Boot on K32L3A

跳至解决方案
1,814 次查看
jraczak
Contributor I

I'm trying to implement secure boot on my project. I'm using the K32L3A and using BLhost to write the IFR's. I seem to have all other functions working except secure boot. For simplicity of testing, I'm putting an unsigned image and not programming the RKTH onto the part. I would like to see it not boot when I enable secure boot. My process is as follows.

  1. Enable secure boot
    1. The command I use is: ./blhost --spi <mysettings> --noping -- flash-program-once 0x98 8 FFFFFF00FFFFFF00
    2. According to this article each bit in the IFR is mapped to a CCOB register and the register should be written with a 0xFF for b'1 and 0x00 for b'0. I should be writing 11101110 to the register, which according to the documentation is:
      • secure boot enabled.
      • secure boot development mode disabled
      • if secure boot fails, go to bootloader mode.jraczak_0-1715198758152.png
  2. Enable Flash security.
    1. The command I use is: ./blhost --spi  <mysettings> --noping -- flash-program-once 0x80 4 FFFFFFFF
    2. I'm very confident this command works because any subsequent BLHost commands get a response of "security must be disabled".

 

Upon reset, the unsigned image boots, meaning secure boot is not active. I can't find any examples of how to enable secure boot and based on the user guide, these seemed to be the only two necessary steps. Any help is appreciated!

 

 

0 项奖励
回复
1 解答
1,739 次查看
jraczak
Contributor I

I was able to solve the issue. 0xFF and 0x00 only maps to logic 1's and 0's for some of the IFR's. It turns out, I just had to use ./blhost --spi <mysettings> --noping -- flash-program-once 0x98 8 FFFFFFFFFFFFFFE1 to get my desired setting.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,740 次查看
jraczak
Contributor I

I was able to solve the issue. 0xFF and 0x00 only maps to logic 1's and 0's for some of the IFR's. It turns out, I just had to use ./blhost --spi <mysettings> --noping -- flash-program-once 0x98 8 FFFFFFFFFFFFFFE1 to get my desired setting.

0 项奖励
回复
1,783 次查看
bobpaddock
Senior Contributor III
Is there any Endian byte swapping going on? That would not be apparent in writing all 0xFFs, it would in real data.

M0+ are Little Endian.
0 项奖励
回复