How to Enable Secure Boot on K32L3A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Enable Secure Boot on K32L3A

ソリューションへジャンプ
2,044件の閲覧回数
jraczak
Contributor I

I'm trying to implement secure boot on my project. I'm using the K32L3A and using BLhost to write the IFR's. I seem to have all other functions working except secure boot. For simplicity of testing, I'm putting an unsigned image and not programming the RKTH onto the part. I would like to see it not boot when I enable secure boot. My process is as follows.

  1. Enable secure boot
    1. The command I use is: ./blhost --spi <mysettings> --noping -- flash-program-once 0x98 8 FFFFFF00FFFFFF00
    2. According to this article each bit in the IFR is mapped to a CCOB register and the register should be written with a 0xFF for b'1 and 0x00 for b'0. I should be writing 11101110 to the register, which according to the documentation is:
      • secure boot enabled.
      • secure boot development mode disabled
      • if secure boot fails, go to bootloader mode.jraczak_0-1715198758152.png
  2. Enable Flash security.
    1. The command I use is: ./blhost --spi  <mysettings> --noping -- flash-program-once 0x80 4 FFFFFFFF
    2. I'm very confident this command works because any subsequent BLHost commands get a response of "security must be disabled".

 

Upon reset, the unsigned image boots, meaning secure boot is not active. I can't find any examples of how to enable secure boot and based on the user guide, these seemed to be the only two necessary steps. Any help is appreciated!

 

 

0 件の賞賛
返信
1 解決策
1,969件の閲覧回数
jraczak
Contributor I

I was able to solve the issue. 0xFF and 0x00 only maps to logic 1's and 0's for some of the IFR's. It turns out, I just had to use ./blhost --spi <mysettings> --noping -- flash-program-once 0x98 8 FFFFFFFFFFFFFFE1 to get my desired setting.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,970件の閲覧回数
jraczak
Contributor I

I was able to solve the issue. 0xFF and 0x00 only maps to logic 1's and 0's for some of the IFR's. It turns out, I just had to use ./blhost --spi <mysettings> --noping -- flash-program-once 0x98 8 FFFFFFFFFFFFFFE1 to get my desired setting.

0 件の賞賛
返信
2,013件の閲覧回数
bobpaddock
Senior Contributor IV
Is there any Endian byte swapping going on? That would not be apparent in writing all 0xFFs, it would in real data.

M0+ are Little Endian.
0 件の賞賛
返信