請問如何修改 S32144 linStack LDF File path

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

請問如何修改 S32144 linStack LDF File path

267 Views
WatsonHsu
Contributor I

請問如何才能修改 S32144 linStack LDF File path,

我的IDE 版本如下:

WatsonHsu_4-1744774402136.png

 

在此版本的 LDF File 後面並無選擇 LDF 路徑方式 (無 "..." , 只能在 SDK 固定路徑下, 在此固定路徑下我已經有放LDF_D31.ldf 所以沒有報錯)

WatsonHsu_0-1744773805688.png

如果我將我的  LDF File 放在source code 下 Function\LDF_D31.ldf , 並將LDF FIle 路徑改為圖中的方式,, IDE 便會報路徑錯誤 

WatsonHsu_3-1744774255534.png

請問要如何才能修改 LDF File 路徑到我希望的位置 , 要不然 source code 

會與 LDF File 分開造成source 管理不便. 謝謝!!

0 Kudos
Reply
5 Replies

220 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @WatsonHsu,

Please refer to the release notes of the SW.

LINSTACK 1.0.1 is compatible with S32DS 3.4 and RTD 1.0.1

danielmartynek_0-1744873547998.png

LINSTACK 1.0.0 is compatible with S32DS 3.4 and RTD 1.0.0 hotfix 01

danielmartynek_1-1744873575889.png

I would recommend having one S32DS IDE that has just one RTD and its compatible extensions installed.

It is possible to install more S32DS IDEs if needed for other RTD versions.

 

Regards,

Daniel

 

 

 

0 Kudos
Reply

243 Views
WatsonHsu
Contributor I

Thank for your help.

My S32 IDE Version is 

S32 Design Studio for S32 Platform
Version: 3.4
Build id: 201217 (Update 3)

I didn't find LInstack software in Install software, (Should I install Linstack again by myself ?)

WatsonHsu_0-1744852669021.png

But I find LIN_stack_S12_4_6_6 in by NXP folder (maybe NXP IDE V3.4 auto install, I did't install Lin Stack)

WatsonHsu_3-1744853282800.png


I can't find the checkbox "support LDF Absolute path" 

WatsonHsu_2-1744853051399.png 

 

 

0 Kudos
Reply

253 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @WatsonHsu,

Which version of the S32K1xx LIN STACK do you use?

danielmartynek_0-1744806245512.png

In LINSTACK 1.0.1, there is this option to select an absolute path to the LDF:

danielmartynek_1-1744806359167.png

 

Regards,

Daniel

0 Kudos
Reply

234 Views
WatsonHsu
Contributor I

I had install LINSTACK S32K1 1.0.2 in my S32 Designe studio,

WatsonHsu_0-1744869321728.png

but the middleware still 1.0.0 

WatsonHsu_1-1744869364702.png

 

 

0 Kudos
Reply

236 Views
WatsonHsu
Contributor I

I fonud my platform.middleware.linstack 1.0.0 ,
Cloud you tell me what is your version  and S32 Design Studio for S32 Platform Version  ? Thank!!

WatsonHsu_0-1744856625575.png

 

0 Kudos
Reply