TJA1443A无法进入Listen-only或者sleep等其他模式

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1443A无法进入Listen-only或者sleep等其他模式

554件の閲覧回数
harryoceana
Contributor II

MCU: s32k344  使用TJA1443A

RTD3.0.0

1. 我将TJA1443A的stb和en引脚拉高,可以正常收发数据,但是我将stb引脚拉高en引脚拉低,外接的can卡无法向总线发送数据,S32K344的CAN中断也没有进入。应该怎么才能正确进入Listen-only模式呢?

2. TJA1443A sleep的情况下,外接CAN卡是否能够发送数据成功,假设总线只有这两个设备,有终端电阻

0 件の賞賛
返信
1 返信

515件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI 

从nomral 跟standby模式进入listen only的条件是一样的请看下面:

你要确认进入listen only之前的状态是什么,然后再判读是否进入listen only模式:

A HIGH level on pin STB_N and a LOW level on pin EN selects Listen-only mode,
provided VBAT and VIO are present. Pin INH remains HIGH, so voltage regulators
controlled by pin INH will also be active.
In Listen-only mode the receiver is enabled, but the transmitter is disabled.

guoweisun_1-1747016735524.png

2:In Sleep mode, the transceiver behaves as described for Standby mode, with the
exception that pin INH is set high-ohmic.

In Standby Mode the TJx1443 is not capable of transmitting and receiving regular CAN
messages, but it monitors the bus for CAN messages.

是无法收发CAN信息的在sleep下。

 

0 件の賞賛
返信