imx-image-hovergames build failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-image-hovergames build failure

Jump to solution
2,315 Views
bschuste
Contributor II

Hi,

I followed the instructions from https://github.com/NXPmicro/meta-nxp-hovergames README file.

On ubuntu 18.04, running the command bitbake imx-image-hovergames ends with the following error:

ERROR: imx-boot-1.0-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1162"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/brigitte/imx8/hovergames/sources/poky/scripts:/home/brigitte/imx8/hovergames/build/tmp/work/imx8mmnavq-poky-linux/imx-boot/1.0-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/brigitte/imx8/hovergames/build/tmp/work/imx8mmnavq-poky-linux/imx-boot/1.0-r0/recipe-sysroot/usr/bin/crossscripts:/home/brigitte/imx8/hovergames/build/tmp/work/imx8mmnavq-poky-linux/imx-boot/1.0-r0/recipe-sysroot-native/usr/sbin:/home/brigitte/imx8/hovergames/build/tmp/work/imx8mmnavq-poky-linux/imx-boot/1.0-r0/recipe-sysroot-native/usr/bin:/home/brigitte/imx8/hovergames/build/tmp/work/imx8mmnavq-poky-linux/imx-boot/1.0-r0/recipe-sysroot-native/sbin:/home/brigitte/imx8/hovergames/build/tmp/work/imx8mmnavq-poky-linux/imx-boot/1.0-r0/recipe-sysroot-native/bin:/home/brigitte/imx8/hovergames/sources/poky/bitbake/bin:/home/brigitte/imx8/hovergames/build/tmp/hosttools"; export HOME="/home/brigitte"; git -c core.fsyncobjectfiles=0 remote failed with exit code 128, output:
fatal: not a git repository (or any of the parent directories): .git

ERROR: imx-boot-1.0-r0 do_fetch: Fetcher failure for URL: 'git://source.codeaurora.org/external/imx/imx-mkimage.git;protocol=https;branch=imx_5.4.24_2.1.0'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/brigitte/imx8/hovergames/build/tmp/work/imx8mmnavq-poky-linux/imx-boot/1.0-r0/temp/log.do_fetch.13442
ERROR: Task (/home/brigitte/imx8/hovergames/sources/meta-imx/meta-bsp/recipes-bsp/imx-mkimage/imx-boot_1.0.bb:do_fetch) failed with exit code '1'

 

What could possibly be wrong?

Thanks,

Brigitte

 

0 Kudos
1 Solution
2,308 Views
bschuste
Contributor II

 

Defining these git parameters solved the problem:

git config --global user.email "<first.last@example.com>"
git config --global user.name "<First Last>"

Needed to clean the current state with command first:

bitbake -c cleanall imx-image-hovergames

 

View solution in original post

0 Kudos
2 Replies
2,300 Views
iaingalloway
NXP Employee
NXP Employee

Thanks for posting this issue and the solution!
Indeed the first time you use git it must be configured to have your username and email 

0 Kudos
2,309 Views
bschuste
Contributor II

 

Defining these git parameters solved the problem:

git config --global user.email "<first.last@example.com>"
git config --global user.name "<First Last>"

Needed to clean the current state with command first:

bitbake -c cleanall imx-image-hovergames

 

0 Kudos