What is the parameter SENS_EN_LL40LS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the parameter SENS_EN_LL40LS?

跳至解决方案
1,814 次查看
nxf58541
NXP Employee
NXP Employee

In QGroundControl, if I see 'SENS_EN_LL40LS' under Parameters --> Sensors, does that mean it's enabled in the firmware? Or, do I need to build the firmware with it included?

0 项奖励
1 解答
1,762 次查看
nxf58541
NXP Employee
NXP Employee

SENS_EN_LL40LS is a parameter to enable the Lidar Lite driver in PX4. This should be part of the distance sensor driver that is part of the standard firmware build for FMUK66.

在原帖中查看解决方案

0 项奖励
1 回复
1,763 次查看
nxf58541
NXP Employee
NXP Employee

SENS_EN_LL40LS is a parameter to enable the Lidar Lite driver in PX4. This should be part of the distance sensor driver that is part of the standard firmware build for FMUK66.

0 项奖励